AnsweredAssumed Answered

ADV7611

Question asked by carlV on Oct 7, 2013
Latest reply on Oct 7, 2013 by mattp

hi

 

the HDMI1.3 and 1.4 and supports TMDS link with speeds up to 3Gb / s, which gives a maximum frequency of 300 MHz normally. However, the ADV7611 is available with a maximum frequency of 80 MHz. But in the datasheet they talk about 162.5 MHz, which is more reasonable.

http://www.analog.com/static/imported-files/data_sheets/ADV7611.pdf

But he may be a doubt about the mode DDR / SDR there.

 

thanks

regards

Carl

Outcomes