AnsweredAssumed Answered

Blackfin being connceted to 2 SPI flash modules via SPI#0

Question asked by Sentinel on May 31, 2010
Latest reply on May 31, 2010 by vapier

I would like to connect 2 SPI flash modules via SPI#0 in a parallel manner, where the SPI flashes will be selected by CS0 and CS1.

The capacity of each flash is 128Mbit.

SPI#1 and SP#2 are active too for another purpose.

 

1) Is it possible?

2) What is the max flash capacity that supported in such connection?

Outcomes