AnsweredAssumed Answered

looking for reference circuit of AD9834 to op amp

Question asked by DanMez on Sep 30, 2013
Latest reply on Oct 4, 2013 by DanMez

Am trying to build a function generator that will be used in a material test system.  The output will vary across a wide range of levels and frequencies, so have been looking at the application note CN0156 which uses the FS Adjust input of the AD9834 to control the amplitude, that could work well.  This would then need to go to an op amp to deliver some power.  I just need a clean sine, not square or other waves.

 

Are there any reference circuits available that have any similar DDS part with output to an op amplifier?  The wide range of frequencies from .1 to >30 MHz might make the op amp selection a little challenging, but since this is like a standard function generator, maybe there are some reference circuit examples available.  Does anyone know of any?

 

Thanks,

Dan

Outcomes