AnsweredAssumed Answered

XTALP and XTALN of ADV7611.

Question asked by Tamu on Sep 30, 2013
Latest reply on Oct 3, 2013 by GuenterL

Hello.

 

I have a question about XTALP and XTALN of ADV7611.

There is a description on the Hardware User Guide, 19 page as follows:
"The ADV7611 supports 27.0, 28.63636, 24.576, and 24.0 MHz frequency crystals. "

 

Even if we use any of the four frequency, I think that the performance of ADV7611 is same.
(For example, I think there is no different performance between when we use 27.0MHz and when we use 28.63636 MHz.)
Is this right?

 

Thank you!
Best regards.
Tamu

Outcomes