AnsweredAssumed Answered

ADP2108 Quiescent Current Question

Question asked by Jacky-chen-2 on Sep 30, 2013
Latest reply on Oct 3, 2013 by LucaV

Dear All:

I tested ADP2108-3.3-EVALZ and ADP2108UJ-3.3-EVALZ Evaluation Board to found if Vin=3.43V/Vout:Non-load now quiescent current is 3.4mA,but Vin=3.65V/Vout:Non-load quiescent current is 41uA, Why is there such as situation? It's the IC's character? can you provide suggestion to me? thanks

 

I needs: (A):uA quiescent current, (B):High power efficiency, (C):Vin:3.4V/Iout=500mA then Vout need keep 3.2V (Before I tested ADP2370 Fail) ,I actually test TI TPS62291 there can meet my requirements.

 

Test platform building:

 

Test Case 1:Vin=3.43V, Vout:Non-load, DSO display: L1(Suspected PWM Mode), Test Result:Vin quiescent current = 3.404mA

 

image002a.jpg

 

 

Test Case 2:Vin=3.65V, Vout:Non-load, DSO display: L1, Test Result:Vin quiescent current = 41uA

image001a.jpg

 

 

Best Regards,
Jacky

Outcomes