AnsweredAssumed Answered

Audio input lost!

Question asked by AzEd on May 24, 2010
Latest reply on May 26, 2010 by JeradL

Using ADAU144x development board.  Numerous edits and additons all resulting in successful compile, link and downloads.

 

After an edit with successful link, compile and download, there is no audio in.  Loading other exiating files are ok - there is audio.  Reloading "problem file" and removing everything except the input and output (direct wire), audio output still fails.  Adding another IC, to the "problem" file, with just an input an output works ok.

 

Is there a way to recover from this as the design is large?  Currenlty using 70% of the available instrction space and 80% of the MIPS.

 

I had this happen before and a block by block cut/pate to a new file fixed the issue...

 

/ed

Outcomes