AnsweredAssumed Answered

DMA external port of shrac 21489  cash reboot

Question asked by eagles on Sep 25, 2013
Latest reply on Oct 1, 2013 by Harshit.Gaharwar

Hi,

     I run a standard DMA on the external port of sharc 21489 (external memory devices -> internal memory).

I encountered two problems in the process of DMA implement .


First ,I set up the dma transfers at the Interrupt handler(IRQ1) ,after IRQ1 interrupt execution ends, the system will be reboot .

 

Then,I set up the dma transfers at the main task(whihout operating system) .

Strangly, the length of ICEP/ECEP register can not be equal or greater than 144 bytes, Otherwise the system will be reboot .

 

When system reboot after an crash occurs, I can not find any useful messagle to locate the crash.

 

Reagrds.

    eagle

 


Outcomes