AnsweredAssumed Answered

HP-USB-ICE Emulator set breakpoints for TigerSharc Multiproc system

Question asked by Chesterfild on May 27, 2010
Latest reply on Jun 9, 2010 by CraigG

Hy Everybody,

 

Sorry for starting a new thread for this, but I would have another question in  connection with setting breakpoints during emulation.

Now I have a hardware makeup, which consists of two TigersharC processors which don't use common memory, and they use link port for communication with each other.

I have a project  consists of many asm and C source files, and tow main functions since it is a multiprocessing system. I'd like to debug during emulation, which for I use an HP-USB-ICE Emulator.  Now  I'm able to set breakpoints in the source window (and both in the disassembly window) during emulation, but  not everywhere I wanted.

Now the situation is the following:

After I build and load my project to the emulator, I can see that the two main files  (maindsp0.c, and maindsp1.c) are visible in my source window as: DSP A (ID0): maindsp0.c, and DSP B (ID1): maindsp0.c . Now I am avaliable to set breakpoints in the source window, but only for this two main files, in other asm or c source files I cannot, there ara no error messages or warnings or anything else, simply nothing happens.. But If I run the program, and I halt it, I can see that other source files are "loaded to or something" to the DSP-s, these soure files jump up in the source window, and they will be named similarly like like the main file-s (for example: DSP A (ID0): brcFAN.asm ). And then I can set breakpoint in these files to, but only in these, which are "loaded".

 

So my question would be: How can I set breakpoints in any files of my project in the source window, before I'm steping into these files during run? I could use some explanation araound breakpoints:)

 

Thank you very much for your answers!

Regards,

Chester

Outcomes