AnsweredAssumed Answered

SPI Emulation using SPORTs  (adsp-21469)

Question asked by alessio on May 26, 2010
Latest reply on Jun 8, 2010 by alessio

Hello,

 

is it possible to emulate full-duplex SPI communication via SPORTs?

 

I have already dedicated 2 available SPI ports as SPI masters.

I need additional SPI slave. I guess if this is possible I would need

2 SPORTs for this job (which I do have available).

 

The emulated SPI via SPORT on adsp-21469 will be used as a slave

to communicate with additional microcontroller (used as SPI master).

 

I read EE-244 and EE-248 and didn't find a way for full-duplex SPI communication there.

Does somebody has any example or pointers how to proceed?

 

Thanks,

~Aleš

Outcomes