AnsweredAssumed Answered

Can I use one single AD1938 for 8 mono outputs?

Question asked by 3dB on Sep 20, 2013
Latest reply on Sep 23, 2013 by 3dB

I'm working on a multichannel audio device that needs 2 Stereo inputs and 8 Mono outputs.

 

My first choice was AD 1939 but I luckily realized that the DAC's are configured as differential pairs and just 4 mono outputs...

 

So, the question is: Can I use the AD 1938 that has 8 single end outputs to get 8 independent mono outputs?

And if so (I ask this in behalf of the SW guy who does the programming...): In what mode? I guess that it has to be done in TDM mode?

Outcomes