AnsweredAssumed Answered

The 2011 release compilation

Question asked by vrp on Sep 11, 2013
Latest reply on Sep 18, 2013 by vrp

I have installed a new openSUSE 12.3, all  latest packages using `sudo`, and ncurses.

 

Then  i have installed:

 

blackfin-toolchain-2011R1-RC4.x86_64.rpm

blackfin-toolchain-uclibc-default-2011R1-RC4.x86_64.rpm

 

and have set the PATH:

 

export PATH=$PATH:/opt/uClinux/bfin-uclinux/bin:/opt/uClinux/bfin-linux-uclibc/bin

 

After unpacking blackfin-linux-dist-2011R1-RC3.tar.bz2

in `make menuconfig` I have chosen BF537-STAMP.

 

Compilation of the kernel was rather long, and then an error appeared:

 

make[5]: Entering directory `/home/pvr/Documents/blackfin-linux-dist/lib/ncurses/build-host-ncurses-5.7/progs'

cc ../objects/tic.o ../objects/dump_entry.o  -I../progs -I/home/pvr/Documents/blackfin-linux-dist/lib/ncurses/ncurses-5.7/progs -DHAVE_CONFIG_H -I/home/pvr/Documents/blackfin-linux-dist/lib/ncurses/ncurses-5.7/progs/../include -I. -I../include  -D_GNU_SOURCE -DNDEBUG -O2 -g  --param max-inline-insns-single=1200 -static -L../lib -lncurses -L../lib -lncurses -dynamic   -o tic

/usr/lib64/gcc/x86_64-suse-linux/4.7/../../../../x86_64-suse-linux/bin/ld: cannot find -lc

collect2: error: ld returned 1 exit status

make[5]: *** [tic] Error 1

make[5]: Leaving directory `/home/pvr/Documents/blackfin-linux-dist/lib/ncurses/build-host-ncurses-5.7/progs'

 

What should I correct?

Outcomes