AnsweredAssumed Answered

use ADV7511 to convert RGB input to HDMI Output

Question asked by StefanoM-Live on Sep 10, 2013
Latest reply on Sep 11, 2013 by DaveD

Hi

 

We are planning to use ADV7511 to convert RGB input to HDMI Output.

In particular we use iMX28, 16 bit LCD controller outputs, and IIS Audio from a dedicated Audio DSP

 

Input RGB Spec :

-RGB 565 ( 16 bit )

-Resolution 800 x 480, @60Hz

 

My question is can we convert this signal to HDMI 1920 x 1080 ?

If yes, buying the EVAL-ADV7842-7511P ev Board can I input the RGB + Sync and Audio Signals thru any connector eventually present on the board, in order to check before building custom board ?

 

Thank you

Outcomes