AnsweredAssumed Answered

ADV7403 Script Error when first running

Question asked by blufocus on Aug 14, 2013
Latest reply on Aug 16, 2013 by tsweeney

I just installed the software for the ADV7403 board.  When I connect the board and run the application I receive the following error messages:

 

There is no  ADV7341.set file in the Default Folder, as there should be in order for the selected script to function.

Please Select a different script or put the correct .set file  in the folder before trying to select the script.

Click on  Show Defaults to view which .set files are in the Defaults Folder.

 

In the C:\Program Files (x86)\ADV Register Control 3.56\Defaults I have the following files:

 

ADV7341B.set

ADV7403.set

ADV7403@.set

 

Additional details: in the C:\Program Files (x86)\ADV Register Control 3.56\Setup_Files folder, I have the following files:

 

adv_config.txt

ADV7403_ADV7403@_ADV7341-VER.1.3.txt

 

Any information anyone can provdie me is greatly apprecaited.

 

Best,

Juan

Outcomes