AnsweredAssumed Answered

unable to read uramdisk.image.gz - ZC702-ADV7511-SDK14.4

Question asked by anupkini on Aug 12, 2013
Latest reply on Aug 26, 2013 by larsc
Branched to a new discussion

hi All,

 

I am trying to bring up Linaro on the ZC702 with HDMI display.

I get the following error msg

 

U-Boot 2013.04 (Aug 05 2013 - 14:42:23)

 

 

I2C:   ready

Memory: ECC disabled

DRAM:  1 GiB

WARNING: Caches not enabled

MMC:   zynq_sdhci: 0

SF: Unsupported manufacturer 00

*** Warning - spi_flash_probe() failed, using default environment

 

 

In:    serial

Out:   serial

Err:   serial

Net:   Gem.e000b000

Hit any key to stop autoboot:  0

Copying Linux from SD to RAM...

Device: zynq_sdhci

Manufacturer ID: 1b

OEM: 534d

Name: 00000

Tran Speed: 50000000

Rd Block Len: 512

SD version 3.0

High Capacity: Yes

Capacity: 7.5 GiB

Bus Width: 4-bit

reading uImage

2918616 bytes read in 485 ms (5.7 MiB/s)

reading devicetree.dtb

10091 bytes read in 17 ms (579.1 KiB/s)

reading uramdisk.image.gz

** Unable to read file uramdisk.image.gz **

zynq-uboot>

 

 

 

I have taken the latest ADI reference designs and linux adi server today.

I am using the 14.4 SDK to build the BOOT.BIN file.

 

Let me know if anyone has faced a similar issue or knows a solution.

 

 

Thanks,

Anup.

Outcomes