AnsweredAssumed Answered

ADV7611 with Micro HDMI

Question asked by conrad.wang on Aug 9, 2013
Latest reply on Aug 12, 2013 by GuenterL

Hello all,

 

I'm currently using the ADV7611 with a micro HDMI connector (type D HDMI connector). The micro HDMI cable that is inserted fits loosely in the connector and allows for quite a bit of movement (It seems like a loose fitting cable is a common complaint with regards to the micro  HDMI interface). When I wiggle the cable around moving it back and forth between the left and right extremes it causes pin 64 on the ADV7611 (RXA_5V) to short to ground inside the chip, thus pulling the +5V supply low. Has anybody experienced this before? I'm thinking it could be pins shorting at the cable and the connector.

 

Thanks,

Conrad

Outcomes