AnsweredAssumed Answered

7619 Minimum Pixel Clock rate for 2 x SDR 4:4:4 Interleaved output

Question asked by rhb on Aug 7, 2013
Latest reply on Aug 8, 2013 by GuenterL

The 7619 includes interleaved pixel output modes for pixel clocks above 150 MHz, such as "2 x SDR 4:4:4 Interleaved" mode - where the pixel output is 48b wide at 1/2 of the incoming pixel clock rate.

 

Is there a minimum pixel clock rate for these interleaved modes? 

 

For example - is it possible to take in a 100 MHz pixel clock and use the 2 x SDR 4:4:4 mode resulting in an output clock (LLC) of 50 MHz?

Outcomes