AnsweredAssumed Answered

ICE100B bug after load a program

Question asked by jaime.of on Aug 7, 2013
Latest reply on Aug 7, 2013 by CraigG

Hi,

 

I am having troubles after loading an image in a Blackfin. The process until get the error is:

1.- Test the program on the board using the emulator and it runs properly.

2.- Generate .dxe file.

3.- Write the .dxe file in the flash memory,

4.- Reset the system.

 

After reset the system, the program is not running (the power consumption decreases) and it is not possible to connect with the DSP using the ICE100B. Before the reset, it is possible to connect with the DSP and it is possible to program it again. The messages that I obtain are the following:


ErrorType.JPG

ErrorMessage.JPG

What is the problem? Maybe the ICE100B is not working?


Outcomes