AnsweredAssumed Answered

AD9129 widebande performance

Question asked by RF_MAN on Aug 5, 2013
Latest reply on Nov 22, 2013 by danf

Hi,

 

I want to use the AD9129 for a wideband design (20 up to 2200MHz ), in the datasheet, the figure 155 give the Pout in frequency vs theorical curves.

- Which of the two recommended circuit is used for these figure ? (Figure 152 or Figure 154) ?

 

- In case what is the response of the circuit in Figure 154 in "normal mode"

 

- In any way I want to buy a demo-board before designing the board, and I think about ad9129-mix-ebz, but is it possible to use the AD-DAC-FMC-ADP adapter board (the documentation talk about the ad9129-ebz only).

 

Thanks for your response.

Outcomes