AnsweredAssumed Answered

CCES request -- incremental build following exclusion of file

Question asked by MikeSmithCanada on Jul 24, 2013
Latest reply on Jul 24, 2013 by MikeSmithCanada

How do I set the build settings to handle this.

 

I have a project with 70 files (literally).  I F7 to build

One file.cpp has wrong syntax -- I fix and rebuild -- only the one file rebuilss as should occur with an incremental build

 

After working overtime until 3 am  :-)  I decide that I am never going to fix the problem

So I exclude the file.cpp and the file-calling.cpp files from project

System now rebuilds all 68 files not just the ones excluded

Found (because I am tired) that I never actually excluded the file-calling.cpp file from the project -- I exclude it --

again system now rebuilds all 68 files not just the ones excluded

 

Since I am hunting down a weird error in 5 files and am including and excluding files for this large project 30 times an hour, then a total rebuild is time consuming

 

Obviously -- the system is enforcing a clean all following an inclusion or an exclusion of a file (or moving a file from one project folder to another)

 

How do I over-ride that -- tried various things -- but did not work

 

Thanks

Outcomes