AnsweredAssumed Answered

Error -- No processor information found

Question asked by MikeSmithCanada on Jul 22, 2013
Latest reply on Jul 23, 2013 by CraigG

I have a CCES 21469 project that is giving me this error message

 

Loading application: "E:\Research\uTTCOS_Backups\VDSP2013_TTCOSLibraryBuild\ADSP21469Specific\SHARC21469_uTTCOS2013_LibBuilder\Debug\SHARC21469_uTTCOS2013_LibBuilder.dxe"

No processor information found; assuming ADSP-21469.

Load complete.

 

The board has existing code that flashes the LEDS -- when I download the code -- the flash temporarily stops -- indicating that something is happening over the emulator -- but then the flashing restarts

 

I have break points in the code -- but they don't get reached -- indicating to me that the code is not really running.

I can download other projects to the boaard -- no problems

I have cleaned rebuilt, rebooted HPUSB-ICE and board and then the whole system

I can force the project to ask me about hooking up to the board -- select processor and emulator

 

I even went and changed the main to be this

#include <stdio.h>

 

void main(void) {

    printf("Hi there\n");

}

 

No luck.

 

This was an imported original VDSP project -- so I think I will just delete the CCES port directories -- reboot the system and reconvert it

However, before I do that -- anything you would like me to examine

Outcomes