AnsweredAssumed Answered

Missing link for CCES  SHARC download package

Question asked by MikeSmithCanada on Jul 21, 2013
Latest reply on Jul 22, 2013 by CraigG

At

http://download.analog.com/tools/SWExamples/all_examples.html#EZKSW15

 

there is a link for a support package

 

 

ADSP-21469 EZ-KIT Lite® Board Suppport Package Rel.1.0.0

256_Point_FFT

This project performs 256 point FFT.

Sharc

ADSP-21469

512_Point_FFT

This project performs 512 point FFT.  The input is given from inputcomplx.dat file.  The output can be compared with the Matlab generated output FFT512complx.dat. Since the FFT accelerators work with 32 bits the output will be rounded. The 512point FFT is split into 32*16(V*H) matrix V =32, H = 16.

 

However that link does not seem to provide a download but goes to

http://www.analog.com/en/evaluation/21469-EZBRD/eb.html

 

but does not provide a SHARC package -- The link for Blackfin package worked

 

Documentation

 

 

Software and Tools

  •      SHARC Evaluation Kits         
    EZ-KIT Lite evaluation kits provide developers with a cost-effective method for initial evaluation of a SHARC processor via a USB-based PC-hosted tool set.    

 

Outcomes