AnsweredAssumed Answered

CCES replacement for interrupts

Question asked by MikeSmithCanada on Jul 21, 2013
Latest reply on Jul 22, 2013 by CraigG

Hi

 

I am using the CCES option to convert a VDSP ADSP-21469 project -- audio talkthrough program I modified

 

The only error I have is for

#include <signal.h>


interrupts(SIG_SP1, uTTCOS_Update);

 

with CCES compiler saying that interrupts( )  is used without a prototype and SIG_SP1 is not defined

 

I presume that this means I have to take a different approach to interrupts

 

is there a 21469 demo audio talkthrough program already converted to CCES?

The only CCES SHARC examples I can see are No_HW

 

When I moved the Blackfin audio talkthrough  from VDSP to CESS -- the interrupts went over smoothly

 

Thanks

Mike

Outcomes