AnsweredAssumed Answered

Export Automatically?

Question asked by Christopher on Jul 19, 2013
Latest reply on Jul 24, 2013 by wsierra

    I am doing some scripting for SigmaStudio 3.8, and I would love to be able to export (*.params, *.hex, ect.) files eaither through a script, automatically through a setting in SigmaStudio for everytime I compile, or on the call of a method (just some sort of consistant automation), is there any way to do this?

 

Thanks!

- Chris

 

P.s How come it is not possible to get properties as well as set properties through the SigmaStudio Scripting API? If it were possible

I would not have to read the files.

 

P.s.s How come the output on these files is inconsistant, for example: I have two filters in my project F0 and F1, one has the coefficants 2, 1, 3, 2, 1 and the other (F1) 2, 1, 3, 1, 3 however F0 gets recorded twice in *.params and F1 does not get recorded at all, this pattern does not seem very consistant either, sometimes they both get exported or nothing does. Could someone explain this?

Outcomes