AnsweredAssumed Answered

ADAU1701 Self Boot Programming.

Question asked by Boscoe on Jul 19, 2013
Latest reply on Jul 19, 2013 by BrettG

So I want to use the ADAU1701 is self boot mode with external EEPROM. I have got Sigma Studio but I have no idea how to configure it to download the program without an USBi converter. Is it possible to just export the code as a .hex file and write this to the EEPROM  with a basic EEPROM programmer? I find this way of only using the USBi difficult expensive and unnecessary.

 

Basically I want a ADAU1701 in circuit with the EEPROM. I add a jumber so I can write to the EEPROM in circuit then put it back power it and works!

 

How do I use Sigma studio to write to the EEPROM?

 

Thanks

Boscoe

Outcomes