AnsweredAssumed Answered

AD9954 Falling Linear Sweep Mode?

Question asked by sss on Jul 19, 2013
Latest reply on Aug 8, 2013 by LouijieC

Dear All,

 

I check the http://ez.analog.com/thread/8684

 

If start falling sweep , they say it should be set as following,

(ex)

FSYSCLK:100MHz

FTW0:60MHz

FTW1:90MHz

 

Fout is,

Fstart:40MHz

Fstop:10MHz

 

 

As well,

If set as following,

FSYSCLK:400MHz

FTW0:360MHz

FTW1:390MHz

 

Fout is ?

Fstart:40MHz

Fstop:10MHz

Is it working to Fout?, characteristic or not degrade, or similar results?

 

Best Regards,

sss

Outcomes