AnsweredAssumed Answered

could I use PVP on core1 ?

Question asked by roilandtangyu on Jul 15, 2013
Latest reply on Jul 15, 2013 by roilandtangyu

I want to port my ADAS algrithom from core0 to core1, the algrithom run on the core0 use the PVP moudle, it's OK. but when I port the algrithom from core0 to core1, the algrithom run error when the application enable the pvp device by calling the function adi_pvp_Enable(); I look into the adi_pvp_Enable function, i found that when call pGlobalPVPRegs->PVP_CTL |= (uint32_t)ENUM_PVP_CTL_PVPEN; ,the application appears the fallowing error:

A fatal error or exception has occurred.

  Description:   No dispatched handler available for the specified interrupt code.

  General Type:  RunTimeError

  Specific Type: NoDispatchedHandler

  General Code:  0x8

  Specific Code: 0xb

  Error Value:   0x000b0077

  Error PC:      0xffa01402

 

my platform:

BF609-EZBORAD

Outcomes