AnsweredAssumed Answered

Problem in G.729AB codec with SDRAM

Question asked by WymanHuang on May 6, 2010
Latest reply on May 6, 2010 by CraigG

Hi,


I am using ADSP-BF531 controller for my audio application and I have VisualDSP++5.0 with update6. My application is encoding PCM data and decoding serial data into PCM data. Now,when I use the encoding rutines ,part of  the G.729AB software module which is downloaded from the ADI website encounted a problem.If I put the sections which were placed in the L1_CODE before,
         INPUT_SECTIONS($OBJECTS(adi_fast_prio0_code))
         INPUT_SECTIONS($OBJECTS(adi_fast_prio2_code))
         INPUT_SECTIONS($OBJECTS(adi_slow_noprio_code))
into the SDRAM_BANK, the rutines will not create the instance of encoding . Is there any solution to solve this problem? Thanks!
Pls forgive my pool English!

Outcomes