AnsweredAssumed Answered

mcapi in buildroot

Question asked by alen on Jul 9, 2013
Latest reply on Jul 10, 2013 by Aaronwu

Hi, ADI experts

     I'm working on bf609 dual - core communications, the basic situation is this : core0 running Linux system, compiled under Linux ; the core1 is a naked nuclear, the main image processing algorithms, under the cces compiled into dxe ; I've compiled to run on the core1 bf609_mcapi_msg_core1 as requested.dxe file now , put it in the /usr/bin directory on the root file system, and then write a code named cces_msg1.c use to communicate with the core1 , and put it in the buildroot/output/libmcapi/libmcapi-2.0/tests directory, and then do make to compiled build cces_msg, put it in /usr/bin directory on a file system, and the last run linux system on the bf609, and run cces_msg  in the root filesystem, and found it can't run. my error log as follows:

捕获1.JPG

Outcomes