AnsweredAssumed Answered

ADV7511WBSWZ without HDCP keys/HDCP License Requirement

Question asked by ChrisM Employee on Jul 4, 2013
Latest reply on Jul 8, 2013 by DaveD
Can you confirm if the ADV7511WBSWZ is available without HDCP keys, and does not require an HDCP license?
It is desirable to have a part with minimum 3 years product life, with the capability of converting 24bit RGB to HDMI up to 165MHz + I2S (4bit).

If the ADV7511-P and ADV7511WBSWZ are not suitable, is the ADV7513 available without keys and still in production?

Would you suggest any other parts?
Thanks.

Outcomes