AnsweredAssumed Answered

Latch and Timer @ ADM2914-1

Question asked by ulfziemann on Jul 4, 2013
Latest reply on Jul 11, 2013 by Ren

Hello,

 

I have the following use case:

- 4 voltages, 1 is negative.

- LATCH is low (remember over voltage)

- TIMER pin with 8.2nF => ~100ms

During startup the TIMER should not trigger /OV vor 100ms (the negative voltage is a lttle late). But after startup the error condition should immediately trigger an /OV.

 

Is it possible with this part?

 

Regards,

Ulf

Outcomes