AnsweredAssumed Answered

FMCOMMS NO-OS test.h definitions

Question asked by AnalogDiode on Jul 3, 2013
Latest reply on Jul 4, 2013 by DragosB

Hi,

 

In test.h of the no-OS software, could you explain the why numbers "128*1024*1024" and "0x6000000" are there in these defintions respectively:

 

#define DDR_BASEADDR          XPAR_DDR_MEM_BASEADDR + 128*1024*1024

 


#define DDRDAC_BASEADDR      DDR_BASEADDR + 0x6000000

 

 

If I change C_MM2S_BURST_SIZE  in AXI_DMA_1  and AXI_VDMA_1 to 32 ( from the default 16), will the above two definitions change?

 

Thanks!

Outcomes