AnsweredAssumed Answered

CCES: loading file error: Code=0x80047344

Question asked by KevinL Employee on Jul 3, 2013
Latest reply on Jul 4, 2013 by CraigG

Hello,

I am getting an error when loading a program into the BF561 simulator.

I have a simple FIR test program (FIR C program from the examples directory) which I build as a BF609 project. I can successfully load this program into the BF561 Simulator.

 

I wanted to make a simple change to the basiccrt operation so the first step was to bring the basiccrt.s file into the project and build it without any changes:

- Copied C:\Analog Devices\CrossCore Embedded Studio 1.0.1\Blackfin\lib\src\libc\crt\basiccrt.s to the project directory

- Imported this file into the project

- Added '-MDUSER_CRT=basiccrt.doj' to the linker options to designate use of the local crt file

- Project builds successfully, and the map file is very similar to the original map file and reveals the use of the local crt file

 

However, when I try to load this .dxe into the simulator as I had done before, I get this error:(details):

Error in launch sequence

[TpsdkServer] Failed to load file: C:\...\fir_609_CCES\fir_609\Debug\fir_609.dxe [Error: , Code=0x80047344]

 

I have searched thru Help but I can't find any information on this error code. Can anyone explain this code?

Outcomes