AnsweredAssumed Answered

Bug in Peak/RMS limiter

Question asked by J3627 on Jul 3, 2013
Latest reply on Nov 18, 2013 by cbrew

The Peak/RMS limiter in ADAU1702 is supposed to have a Peak Hold, according to the documentation, but it does not:

 

2013-07-03 09_56_32-SigmaStudio Help.png

 

Does the RMSTC field do the same thing as a peak hold?  It can be changed between ms and dB/s, so I'm not sure what dB/s means for a hold.

 

Also, is there a way to see what the peak limiter component is doing?  If I turn the 3 RMS values to maximum, it should essentially disable the RMS component and leave only the peak component working, right?  But if I do this it just behaves like an RMS limiter with the values maxed out.

Outcomes