AnsweredAssumed Answered

AD5290 ±5V Supply operation

Question asked by Mr.K on Jul 3, 2013
Latest reply on Jul 3, 2013 by DRice

I want to confirm the operation voltage of AD5290.

 

The range of the AD5290 power supply is described in the top page of the data sheet with ±10V to ±15V.

In page 17 of the data sheet, there is the following descriptions.

 

" The AD5290 can operate in single supply from +4.5 V to +33 V or dual supply from ±4.5 V to ±16.5 V.

  The AD5290 is functional at low supply voltages such as 4.5 V, but the performance parameters are not guaranteed."

 

In this page, there is describing that it can operate from ±4.5V though the performance are not guaranteed.

 

I will use it in the power supply of ±5V.

If the performance described in the data sheet is not need, can I use supply voltage such as ±5V for AD5290?

Outcomes