AnsweredAssumed Answered

ADV7619 Non-CEA Timings

Question asked by rahul1977 on Jul 3, 2013
Latest reply on Jul 30, 2013 by GuenterL

I have a ADV7619 HDMI Receiver Setup. The problem that i am facing currently is when i drive any of NON CEA Timings not mentioned in the 861D spec the video output is not correct.  I read the user guide of ADV7619 but was unable to find any relevant information on this.

 

The timings that i am facing problem with are as below. These are all non CEA modes. I would like to know if ADV7619 supports all these resolutions/RR and if yes what specific programming needs to be done in the HDMI receiver to drive these timings.

 

1152 x 86475Hz
1152 x 86475Hz
1280 x 102459Hz
1280 x 102459Hz
1280 x 102460Hz
1280 x 102460Hz
1280 x 102475Hz
1280 x 102475Hz
1280 x 96059Hz
1280 x 96059Hz
1280 x 96060Hz
1280 x 96060Hz
1440 x 90060Hz
1440 x 90060Hz
1440 x 90075Hz
1440 x 90075Hz
1600 x 120059Hz
1600 x 120059Hz
1600 x 120060Hz
1600 x 120060Hz

Outcomes