AnsweredAssumed Answered

Frequency Divider

Question asked by MagicRuB on May 3, 2010
Latest reply on May 3, 2010 by JeradL

Is there a module, or combination of modules, which can divide a signal from the frequency generator? My application includes mixing some signals from a sine gen source (or external source) but some of the signals must be in perfect phase so they can not be generated from different frequency gens. For example: I need available a 4 kHz and a 2 kHz sine wave in perfect phase. When summed together it shouldn't get goofy due to phase.

 

I'm using an ADAV1442 eval board but am not committed to that particular part. How is this phase relationship best done in Sigma Studio?

Outcomes