AnsweredAssumed Answered

Input configuration of AD9467-250

Question asked by Jacky on Jun 24, 2013
Latest reply on Jun 28, 2013 by UmeshJ

Sir:

 

In the datasheet of AD9467-250, there are two Differential Transformer - Coupled input Configuration(Figure 51 and Figure 52). One is for Baseband Applications   up to 150 MHz , the other  is  for IF Applications from 150 MHz  to 300  MHz.

 

(1) If I want to design a broad band application that span from 1MHz to 300MHz, how should I design the input configuration ?

 

(2) ADT1-1WT is a 75ohm 1:1 transformer, but in Figure 51 and Figure 52 there is a note that indicate the impedance of the transformer is 50ohm("input Z=50ohm").  Why the input impedance for this transformer is 50ohm here?

 

(3) A single transformer is sufficient to transform a single-ended signal to differential signal. Why Figure51 and Figure52 use two-stage transformers?

 

Thanks

Regards

Jacky

2013-06-24

Outcomes