AnsweredAssumed Answered

The error of converting for AD7657

Question asked by Kaos on Jun 21, 2013
Latest reply on Jun 28, 2013 by Kaos

Dear Sir/Madam,

 

I am studying to design with your 12 AD7657s that have same lot number.

So I met the error problem.

Why is this trouble happen?

Please give me your good advice reason why?

 

Condition:

When I input 10V dc here, your AD7657 converted the result 8111 to 8131digit.

This have higher 50 or 60 digit than a theoretical value.

Also input -10V dc here, the converted result was -8111 to -8131 digit.

And when I put this on high tempereture area, the convert value have higher around 100 digit than a theoretical value.

 

Of cource AD7657 have the positive full scale error +/-0.61%.

This means 2^14 * 0.0061=99digit, correct?

If so, 50 or 60 digit means within the full scale error, and no problem correct?

 

In this case, the reason why is come from Vref drift, I thought.

But Vref come from extrnal source and stable.

At in front of analog input(T/H AMP), there is a buffer OPAMP as voltage follower such as your good OP07.

 

Thanks Kaos

 

 

Outcomes