AnsweredAssumed Answered

ADV7842 decolder in bf609 EZ Board

Question asked by alen on Jun 21, 2013
Latest reply on Jun 24, 2013 by Aaronwu

Hi !  ADI's experts


I am interested in Analog Devices video decoder/encoder chip, p/n ADV7842,and I have configed linux kernel and buildroot used make linux-menuconfig and make menuconfig,my configuration is as follows:

 

first :execute make menuconfig

          Blackfin Processor Options  --->

                   Uncached DMA region (Enable 4M DMA region)  --->

 

second:make linux-menuconfig

          Device Drivers  --->

                 <M> I2C support  --->

                                     I2C Hardware Bus support  --->

                                    <M> Blackfin TWI I2C support

                                    (100) Blackfin TWI I2C clock (kHz)

          Device Drivers  --->

                   <M> Multimedia support  --->

                                 [*]   Media Controller API (EXPERIMENTAL)

                           [*]   V4L platform devices  --->

                                       <M>   Blackfin Video Capture Driver

                                 Encoders, decoders, sensors and other helper chips  --->

                                            < > Analog Devices ADV7183 decoder

                                            <M> Analog Devices ADV7842 decoder

                                            < > ST VS6624 sensor support

                                            < > Aptina MT9M114 sensor support

 

After the build is complete, after the runs on the Board, in the/dev/directory not found video 0 equipment??????

Running log file is as follows

 

Bytes transferred = 16962915 (102d563 hex)

## Booting kernel from Legacy Image at 01000000 ...

   Image Name:   bf609-0.0-3.5.7-ADI-2012R2

   Image Type:   Blackfin Linux Kernel Image (gzip compressed)

   Data Size:    16962851 Bytes = 16.2 MiB

   Load Address: 00001000

   Entry Point:  0029daec

   Verifying Checksum ... OK

   Uncompressing Kernel Image ... OK

Starting Kernel at = 0029daec

console [ttyBF0] enabled, bootconsole disabled

Calibrating delay loop... 989.18 BogoMIPS (lpj=1978368)

pid_max: default: 32768 minimum: 301

Mount-cache hash table entries: 512

devtmpfs: initialized

Blackfin Scratchpad data SRAM: 4 KB

Blackfin L1 Data A SRAM: 16 KB (9 KB free)

Blackfin L1 Data B SRAM: 16 KB (16 KB free)

Blackfin L1 Instruction SRAM: 64 KB (51 KB free)

Blackfin L2 SRAM: 256 KB (256 KB free)

NET: Registered protocol family 16

Blackfin DMA Controller

ezkit_init(): registering device resources

ezkit_init(): request emac pins failed

bio: create slab <bio-0> at 0

SCSI subsystem initialized

bfin-spi bfin-spi.0: master is unqueued, this is deprecated

bfin-spi bfin-spi.0: bfin-spi probe success

bfin-spi bfin-spi.1: master is unqueued, this is deprecated

bfin-spi bfin-spi.1: bfin-spi probe success

usbcore: registered new interface driver usbfs

usbcore: registered new interface driver hub

usbcore: registered new device driver usb

i2c-bfin-twi i2c-bfin-twi.0: Blackfin on-chip I2C TWI Contoller, regs_base@ffc01e00

i2c-bfin-twi i2c-bfin-twi.1: Blackfin on-chip I2C TWI Contoller, regs_base@ffc01f00

pps_core: LinuxPPS API ver. 1 registered

pps_core: Software ver. 5.3.6 - Copyright 2005-2007 Rodolfo Giometti <giometti@linux.it>

PTP clock support registered

NET: Registered protocol family 23

Switching to clocksource bfin_cs_cycles

NET: Registered protocol family 2

IP route cache hash table entries: 1024 (order: 0, 4096 bytes)

TCP established hash table entries: 4096 (order: 3, 32768 bytes)

TCP bind hash table entries: 4096 (order: 2, 16384 bytes)

TCP: Hash tables configured (established 4096 bind 4096)

TCP: reno registered

UDP hash table entries: 256 (order: 0, 4096 bytes)

UDP-Lite hash table entries: 256 (order: 0, 4096 bytes)

NET: Registered protocol family 1

msgmni has been set to 210

io scheduler noop registered (default)

bfin-uart: Blackfin serial driver

bfin-uart.0: ttyBF0 at MMIO 0xffc02000 (irq = 88) is a BFIN-UART

physmap platform flash device: 01000000 at b0000000

physmap-flash.0: Found 1 x16 devices at 0x0 in 16-bit bank. Manufacturer ID 0x000089 Chip ID 0x008821

Intel/Sharp Extended Query Table at 0x010A

Intel/Sharp Extended Query Table at 0x010A

Intel/Sharp Extended Query Table at 0x010A

Intel/Sharp Extended Query Table at 0x010A

Intel/Sharp Extended Query Table at 0x010A

Using buffer write method

Using auto-unlock on power-up/resume

cfi_cmdset_0001: Erase suspend on write enabled

Creating 3 MTD partitions on "physmap-flash.0":

0x000000000000-0x000000080000 : "bootloader(nor)"

0x000000080000-0x000000480000 : "linux kernel(nor)"

0x000000480000-0x000001000000 : "file system(nor)"

m25p80 spi0.1: w25q32 (4096 Kbytes)

Creating 3 MTD partitions on "m25p80":

0x000000000000-0x000000080000 : "bootloader(spi)"

0x000000080000-0x000000200000 : "linux kernel(spi)"

0x000000200000-0x000000400000 : "file system(spi)"

CAN device driver interface

bfin_can bfin_can.0: bfin_can device registered(&reg_base=ffc00a00, rx_irq=47, tx_irq=48, err_irq=49, sclk=125000000)

        DWMAC100

No HW DMA feature register supported

Enhanced/Alternate descriptors

RX IPC Checksum Offload not configured.

stmmac_dvr_probe: warning: cannot get CSR clock

stmmac: probed

eth0: PHY ID 20005c90 at 1 IRQ 0 (stmmac-0:01) active

Initializing USB Mass Storage driver...

usbcore: registered new interface driver usb-storage

USB Mass Storage support registered.

musb-hdrc: version 6.0, ?dma?, otg (peripheral+host)

input: bfin-rotary as /devices/platform/bfin-rotary/input/input0

i2c /dev entries driver

bfin_wdt: initialized: timeout=20 sec (nowayout=0)

dma_alloc_init: dma_page @ 0x02477000 - 1024 pages at 0x07c00000

usbcore: registered new interface driver usbhid

usbhid: USB HID core driver

icc icc.0: initialized

TCP: cubic registered

NET: Registered protocol family 17

can: controller area network core (rev 20090105 abi 8)

NET: Registered protocol family 29

Freeing unused kernel memory: 15320k freed

mmc0: host does not support reading read-only switch. assuming write-enable.

mmc0: new SD card at address e624

mmcblk0: mmc0:e624 SU02G 1.84 GiB

mmcblk0: p1

eth0: device MAC address 02:80:ad:20:31:e8

No MAC Management Counters available

 

 

 

 

BusyBox v1.20.2 (2013-06-09 09:32:39 CST) hush - the humble shell

 

 

root:/> PHY: stmmac-0:01 - Link is Up - 100/Full

 

 

 

 


 

 

Outcomes