AnsweredAssumed Answered

editor view during debugging

Question asked by Jeroen_ on Jun 20, 2013
Latest reply on Jun 27, 2013 by Jeroen_

Hello,

 

I have an project with an BF512 in CCES 1.0.1.0. When I start the debugger the "Step over" and "Step into" buttons are disabled. except "run" I can only use "assembly step into" button. The assembly step button is working and if I look in the Disaaembly window I see the green line and that jumps to the next instruction when I pushed the button. So that's working fine. But I also would like to see the c code I wrote. When I start the debugger in the editor window nothing change. I would expect that there the first file appears and stops by the breakpoint at main. How can I change this? I would like to see the code and use the step functions.

 

Regards,

Jeroen

Outcomes