AnsweredAssumed Answered

What is the best procedure to copy a project and its source files?

Question asked by KevinL Employee on Jun 19, 2013
Latest reply on Jun 20, 2013 by CraigG

Typically in VDSP I start with an example project or existing project and copy it so that I don't corrupt the example that resides in the VDSP install directory. I would like to do the same with CCES. What is the best procedure to copy a project and its source files? I have experimented with the export wizard and I have seen inconsistent behavior depending on where C/C++ source files are located. The result is that the project will not build because it can't locate a source file.

Outcomes