AnsweredAssumed Answered

The AD9910 REF CLK source is turned off, but I still have an output frequency. Why is there an output?

Question asked by DSB Employee on Apr 20, 2010
Latest reply on Apr 20, 2010 by DSB

A customer is using our AD9910 evaluation board, he uses an external signal source to supply a REF CLK. There is output at the DDS's output. But when he disabled the signal source's output, there is still an output at the DDS's output. I used the AD9910EVB to do the test. Agilent's 33250A is used to output 25MHz signal to AD9910 REF CLK input. After disabling the 3250A's output or power off to 33250A, there is a signal still a DDS output. So, I would appreciated if you can give some advice.

Outcomes