AnsweredAssumed Answered

Enabling multiple writebacks for 1701 in SigmaStudio?

Question asked by tesla.man on Apr 16, 2010
Latest reply on May 5, 2010 by tesla.man

When using SigmaStudio to program the self-boot EEPROM for a 1701 how can you enable the multiple write-back feature?

The datasheet explains that the command 0x04 needs to be included in the boot sequence but I cannot work out how to force this from within the software. I guess I may have to edit the hex file directly? If so can anyone show an example of the required modification as I'm a little unclear from the datasheet description.

 

Also, once a write-back is triggered can the 1701 continue uninterrupted or will it reset automatically (or need resetting manually)?

I ask because I'd like to be able to trigger a write-back at any time without any disruption to normal function.

 

Thanks,

Dave.

Outcomes