AnsweredAssumed Answered

VDSP and VisualSourceSafe(VSS) as SourceControl

Question asked by pfeifferc on Apr 12, 2010
Latest reply on Apr 14, 2010 by CraigG

Hi,

i'm working for a while with one project  where VSS is used for sourcecontrol. Works fine but now, a new scenario is requested.

 

I want to create a new project which is based on the same "kernel" sources as in the "motherProject". This files should be take from the original

directory and included into my project. But i want to handle it with VSS too in the VDSP IDE.

Standalone VSS have the option "share to" so i could share this source files to another VSS-Project. And checkIn/Out works well in the VSS-Client.

 

But VDSP dont response with the correct checkout status in "kindProject" if i check out the file in the "MotherProject".

I hope my requirements are clear defined.

 

Is there another way to handle "kernel Files" within two different projects?

 

regards chris

Outcomes