AnsweredAssumed Answered

BF537 Caesar_Cipher // write & read into Flash conflict

Question asked by PedroMonje on Apr 7, 2010
Latest reply on Jun 2, 2010 by PrasanthR

Hello everybody;

 

I am using a BF537E DSP and I am  having some problems writing into the Flash memory of the DSP.

 

I have the drivers from Bluetechnix that are used to write & read from the DSP. Those work correctly when I execute them with the DSP.

 

But now I am having some probems trying to integrate those drivers in my design. The DSP runs a Caesar_Cipher_ThreadType thread that comunicates with an aplication in my PC. In some moment I want to send an order an write some data in the Flash Memory.

 

But I can not compile the program because it appears some errors referring the Read_Flash and Write_Flash function. That is:

 

[Error li1021]  The following symbols referenced in processor 'p0' could not be resolved VisualDSP

 

How can I integrate both programs? Are easier ways to write and read data in flash in bf537?

If anyone can help me, I would be pleased. Thanks

Outcomes