AnsweredAssumed Answered

Crystal Selection

Question asked by parleam08.extc on Feb 26, 2010

Exact 12.288MHz crystal is not available in the nearby market.

 

Can I use a 12.000MHz crystal. Since I am using only the analog input and outputs... it wouldn't matter if the sampling frequency is not exactly 48KHz.

Also would it be ok if I use a 22pF load capacitance crystal.

 

Also should I change the PLL component values?

Outcomes