AnsweredAssumed Answered

BF533 with Ethernenet/TCP-IP and ADV7171

Question asked by Taus on Feb 4, 2010
Latest reply on Feb 8, 2011 by PrasanthR

Greetings,

 

I'm a PHd student and I need to get video from Ethernet and show it in a monitor.

 

My first step was to build a project that gets a RGB image, converts to PAL/NTSC and shows it in the monitor.

 

Now I've built another project that builds Ethernet & TCP/IP. I'm able to receive an image and store it in SDRAM.

 

The problems started when I tried to combine the two projects.

 

I'm using I2C Driver to configure ADV7171 but when I add this driver to the Ethernet & TCP/IP project it doesnt work.


It's really strange, I don't need no call any function. The project doesn't work as soon as I add I2C_BF5xx_rev07.asm.

 

I've tried to alter the I2C driver, I began using timer1 and I've also tried to deactivate its interruption but I had no success.

 

Can someone help??

 

Thanks,
Carlos

Outcomes