AnsweredAssumed Answered

Design of PCB layout

Question asked by parleam08.extc on Feb 5, 2010
Latest reply on Feb 10, 2010 by Gordon

Is there anything specific, which I should consider while making the PCB layout.

My circuit contains of ADAU1701, EEPROM, Filters etc. Everything else other than the processor is available in PDIP package which can be soldered by hand.So, I am thinking of making a breakout board for ADAU1701.

Is there any pin of processor which works at very high frequencies? Or is there any component which needs to be placed near the processor?

Would there be any problems due to the increase in the length of the wires connected to the processor due to the breakout board.

 

Also what all crystals can I connect to the processor other than 12.288MHz

Outcomes