AnsweredAssumed Answered

output executable code files

Question asked by mshearer123 on Feb 1, 2010
Latest reply on Feb 2, 2010 by mshearer123

Hi,

 

I would like to be able to create executable code files, With the idea that I could read them into local memory during runtime and execute.

I have no idea how to go about doing this, or if indeed it is possible.

 

So basically how do i go about outputting a small program such as:

 

#include <ccblkfn.h>

void main( void )

{

    *pFIO2_DIR = 0xFFFF;

    *pFIO2_FLAG_D = 0x0001;

}

 

which i can store in external memory, such as flash, load into main memory when needed and execute.

 

thanks for any advice,

 

Matthew

Outcomes