AnsweredAssumed Answered

ADAU1761 safeload

Question asked by inventis on Jan 26, 2010
Latest reply on Jan 27, 2010 by JeradL

Hello,

in the datasheet of adau1761 in the "SOFTWARE SAFELOAD"

there is a table with the address of safeload ram.

 

I have some trouble to understand the behavior of address 0x0000 " Modulo RAM size"

in the datasheet "Address 0x0000, wich controls the module RAM size is set by SigmaStudio and

is based on the dinamic address generator mode of the project".

 

in a FW implementation what is the value that I have to write in this register?

 

What is the procedure to write a safeload parameter in the ram?

 

Have I to WRITE PARAM and WRITE ADDRESS and WRITE NUMBER OF WORDS ?

Outcomes